Installation of WinCAPS without admin rights

Installation of WinCAPS on Windows Vista or 7 without administrator rights

To install WinCAPS 2011.01 on Windows Vista or 7, you must have administrator rights.

file

If you don't have administrator rights, then an error message is shown.

Your IT systems administrator should be able to install WinCAPS 2011.01 on your Windows Vista or 7 computer.

 

You can of course run WinCAPS directly from the DVD without administrator rights.